Get Current Screen

Capture the current screen image from the oscilloscope and display it in the Oscilloscope application window. Note that this operation captures the current screen image without initiating a new measurement.

If Auto Refresh is enabled, the label on this button changes from "Get Current Screen" to "Start Auto Refresh".
Use the "Start" button to trigger a new measurement prior to capturing a screen image.

 

See Also

Export Screen Shot